Looking for more articles? Check out in the groove, our customer magazine.
As airplane designs focus on flying at higher altitudes and speeds for longer periods, the many hydraulic systems onboard must adapt. Today's conditions can include temperatures above 600°F (315,5°C), temperatures as low as -65°F (-54°C), and pressures up to 5,000 psi (345 bar)
This article was originally published in the August 2020 issue of Fluid Power Journal. It is reposted by permission.
Matching Elastomer Seals to Biofuel Applications
As the world attempts to reduce its dependence on fossil fuels, biofuels are now a reality. Brazil and the U.S. were early adopters of this alternative fuel for transportation but now its use is expanding in Europe, with Germany, France and Spain leading the way.
By Harlan Hart, Technical Manager e-mobility for Trelleborg Sealing Solutions.
Recognising that a specialised sealing solution was needed for e-Mobility applications, Trelleborg Sealing Solutions has developed two new seals that could help noticeably extend the distance travelled by electric vehicles between charges, as Harlan Hart, technical manager, e-Mobility, explains
When Electric Vehicles Take Over
By Jeff Kerns, published in "Machine Design Magazine"
Are supply chains, materials, and drivability of EVs helping or hurting?
First appeared in Machine Design
New Seals Reduce Friction for Electric Vehicle Adoption
By Harlan Hart, Technical Manager e-Mobility for Trelleborg Sealing Solutions, published in "Machine Design Magazine"
Increasing electric vehicles driving range is more than just a matter of batteries and motors.
First appeared in Machine Design
As a matter of flat: The importance of high-quality flat seals in chemical transportation
Reprinted with permission from Bulk Transporter. Find the original article at BulkTransporter.com
Secure Transport of Chemicals - Sicherer Transport von Chemikalien
By Marco Schildknecht, Segment Manager Chemical & Processing Europe, Trelleborg Sealing Solutions
Even when exposed to the most aggressive chemicals, the two sealing materials Isolast J9503 and Isolast J9567 perform very well. They seal reliably under extreme conditions and have a long service life.
This article is in German and was originally published in August 2022 in cav - Prozesstechnik für die Chemieindustrie It is reposted by permission, copyrights are reserved to the publication.
Maximizing wind turbine efficiency through optimized hydraulic sealing
Advanced seal designs that prevent wear, increase service life, and reduce friction can ensure uptime in pitch cylinders and brakes.
This article original ran in Sealing & Contamination Control Tips
Minimizing Equipment Downtime with In-situ Seal Welding Technology
The ideal solution is for completion of any seal repairs or replacements on FPSO vessels to be completed offshore, in-situ, to speed up the process and minimize equipment downtime.
Trelleborg introduces XploR S-Seal
By Eric Bucci, published in "Rubber & Plastics News"
Trelleborg Sealing Solutions recently launched XploR S-Seal and XploR FSSeal, extrusion-resistant elastomers the company developed for demanding high temperature and high-pressure sealing environments in the oil and gas industry.
Trelleborg's tensioner cylinder seals exceed 20-year lifecycle rating
By Mary Gannon
Seals used in offshore rig tensioner cylinders must meet the same rigorous lifecycles as the
cylinders themselves. Because offshore environments are harsh and installation and maintenance
can be difficult, tensioner cylinders must have a 20-year life. That was why, more than 20 years
ago, Trelleborg Sealing Solutions conducted research, determining that its seals could last this
necessary lifecycle.
Perfluoroelastomer (FFKM) elastomers offer exceptional thermal stability, outstanding long-term compression set and almost universal chemical compatibility – delivering long life in the most aggressive of media, including hydrocarbon and aqueous media, common within oilfield applications.
As the oil and gas industry evolves, sealing materials are required to work effectively in more challenging environments. This article details the effects of exposure to water-based hydraulic fluids and High-Pressure/High-Temperature (HPHT) fields on common sealing materials.
Simulations reveal valuable information about Fluid Power Components
This article was originally published in the Fall/Winter 2023 issue of Your World in Motion and is shared with permission from the Canadian Fluid Power Association (CFPA). To learn more about CFPA and to read the full issue at no cost, visit https://cfpa.ca/.
To achieve optimal efficiency, fluid power applications and their sealing components need good friction characteristics and long life to reduce maintenance. Engineering simulations can help original equipment manufacturers (OEMs) succeed in an environment where the demands for efficiency are increasing.
Why stocking standard products pays off for OEM and supplier relationships
By Scott Christensen, originally published by "Sealing & Contamination Control Tips"
Original Equipment Manufacturers (OEMs) and their tier suppliers rely on sealing partners for a wide range of services and capabilities. An experienced and knowledgeable sealing supplier can provide everything from high-quality custom sealing solutions and FEA analysis to online tools and resources for engineers.
All Around the World: Circular Sustainability for Fluid Power
In today’s environmental and economic landscape, it is critical for fluid power component manufacturers and seal suppliers to incorporate sustainable methods into design, manufacturing, and production practices through design thinking for circularity and circular products.
This article was originally published in the November 2022 issue of Fluid Power Journal
Spotlight on Sealing Solutions for Fluid Power and Off-Highway
Ensuring performance in extreme conditions, industrial seals meet unique application needs.
First appeared in Machine Design
No-Leak Zone: The Mighty Mechanical Face Seal
Mechanical Face Seals, also called lifetime seals, floater seals, duo cone seals or toric seals are important to the long-life function of heavy equipment in agriculture, construction and mining.
This article was originally published in the February 2022 issue of Fluid Power Journal. It is reposted by permission.
Advancements in Double-Acting Rotary Seals Prove More Effective
By Beth Figliulo, Fluid power segment manager, published in "Electronic Component News", Dec. 2018
How specialized Rotary Seals are alleviating fluid power pressure build-up for high-speed, high-pressure applications
Modern machinery, equipment and motors fitted with hydraulic cylinders are becoming more powerful, which means that the hydraulic systems therein are increasingly subject to higher operating pressures and temperatures.
The right seal reduces contamination in hydraulic systems
Learn what causes contamination and how to choose seals that protect against it.
Trelleborg Sealing Solutions has developed a unique engineered seal– specifically for use within Central Tire Inflation systems. Turcon® Roto L is the first ever active seal, engineered to only provide sealing when required. Eliminating friction and torque, this extends the seal life of axle systems and can significantly reduce fuel consumption for vehicle operators.
Zero-Leak Wipe Systems Fluid 'Weepage'
Hybrid robots combining hydraulic and electric systems are becoming more common in assembly lines and warehouses. Hybrid hydraulic and electrical designs require special care when specifying hydraulic sealing systems because weepage of even a light coating of hydraulic fluid can negatively affect electrical system performance.
This article was originally published in the February 2022 issue of Fluid Power Journal. It is reposted by permission.
High Modulus Plastics Can Play a Key Role in Off-Highway Vehicles
By Tom Zozokos, Product Line Director, and Beth Figliulo, Fluid Power Segment Manager Americas, Trelleborg SealingSolutions.
Co-injection molding is one technology of interest for those designing hydraulic systems for off-highway use. This allows two polymers to be combined in a single operation to create multiple functions in one component.
This was originally published in OEM Off-Highway.
Boosting performance in hydraulic systems with alternative coatings
By Beth Figliulo and Michael Cook, Trelleborg SealingSolutions.
Taking a holistic approach to sealing solutions in hydraulic systems using chrome alternatives helps engineers achieve optimum function.
Materials for Maximum Wear Ring Performance
Published in "Flow Control", May 2018
Read how Wear Rings can extend the life of a hydraulic system
Processing Q&A: Horizontal mixer sealing with Trelleborg's Caio Beraldo
From mixers and food pumps to valves and fillers, the range of equipment and machinery used in the food, beverage and water industry is diverse. Each has its own set of sealing requirements and understanding these critical components takes expertise.
This article appeared on Processing Magazine’s website
Processing Q&A: Vertical mixer sealing with Trelleborg's Caio Beraldo
Trelleborg's Technical Manager for Food, Beverage and Water, recently connected with Processing to discuss the uses and critical sealing components for vertical mixers.
Selecting the right seals for food and beverage processing
Understanding common seal materials and factors that affect performance can help ensure the seling solution best meets the requirements for the application
Engineered Solutions for Smart Appliances with LSR Processing
The Research and Markets Institute (researchandmarkets.com) projects the global household appliances industry to reach an estimated value of US$ 324.2 billion by 2019. Amongst the major drivers are growing affluence of the middle-class population in emerging markets, higher disposable incomes, and more per capita spent on lifestyle products in increasingly urbanized environments.
Product change without aroma carryover
(Language: German)
Trelleborg Sealing Solutions has partnered with Krones, a specialist in beverage bottling, to analyze the reasons behind unintentional flavor carryover during the filling process. The companies found elastomer sealing components to be a relevant factor in aroma carryover and that the selection of the optimum sealing material is crucial in preventing the transfer of flavors from one filling process to the next.
David Kaley — Trelleborg Sealing Solutions; Edited by Mike Santora
With stainless steel and other metals so predominant in industrial food manufacturing equipment, it may seem unusual to suggest a more significant role for plastic wear rings and bearings. But for a broad range of food production and transportation machines, advanced polymers are an effective way to reduce friction and handle load instead of traditional metal bearings.
Trelleborg Seals help keep food and beverage industry clean
By David Kaley, published in "Rubber & Plastics News"
One of the most important aspects for the food and beverage industry is sterility. Preventing cross-contamination on the plant floor is crucial. Any company creating pieces of equipment needs to adhere to the industry's strict regulations.
Smart Engineering Solutions for Smart Appliances with LSR Processing
By Ursula Nollenberger, published in "appliance DESIGN"
The global household appliances industry is seeing a steady influx of technologically advanced appliances that deliver innovative, smart features to save the user time and make life more comfortable. This article demonstrates the role custom-engineered LSR parts have in this segment.
Device Development Excels in Rapid Development Centers
Design and material choices can have a long-term impact on manufacturing costs and effieciencies for medical device manufacturers. When they work together with experienced component manufacturers from the start of a project, they can save time, reduce costs, and produce premium quality products, while keeping an eye on the goal of a smooth transition to serial production.
Handy medical devices make life easier for people with chronic conditions, and automated dosing systems are gradually replacing regular injections of essential medication. Trelleborg cooperated with WACKER to develop a microinjection pump, the very heart of such devices.
Single-Use Systems: The Future of Biopharmaceutical Processing
Single-Use systems represent the future in biopharmaceutical processing of therapeutic drugs with significant advantages
over traditional reusable stainless-steel systems and partly disposable systems.
Q&A: Reducing the cost of long-term manufacturing
Medical Plastic News spoke with Chris Tellers, Rapid Development Center director, Trelleborg Healthcare & Medical to learn out about the company's recently launched Rapid Development Center in Delano, Minnesota
Motors and More: Achieving Greater Effieciency in Industrial Automation Applications
Originally published on Automation.com
Industrial automation is highly beneficial because it decreases production times, improves quality and increases productivity in a world where
customers expect quick turnaround times.
There is no one-to-one replacement
What opportunities and risks the seal supplier Trelleborg sees in the impending ban on PFAS substances (per- and polyfluoroalkyl substances), which is causing nervousness among manufacturers, processors and users.
This is the way—to safe chemical transport
By Thijs Menzel. Reprinted with permission from Bulk Transporter Magazine. Find the original article at BulkTransporter.com
Chemical compatibility, material testing, root cause failure analysis among the critical keys to success, sealing expert says
The right seals and materials keep chemicals moving
ByThijs Menzel
The world relies on chemicals to provide the essentials of modern life and they are the basic building blocks of everyday items; from the fertilizers that help grow our food to the beds we lie on, from the shoes on our feet to the cars that we drive. Transporting those chemicals safely to where they are needed, is a major logistical effort that requires advanced sealing technology.
Biolubricants & Seals: Users and their providers need to pay attention to fluid compatibilities
By Joe Savina, published in "Processing Solutions"
Biolubricant use is on the rise as companies look for more sustainable ways of doing business. Read this article to find out more about the special design considerations required due to how these lubricants may react to equipment components and seal materials.
The chemical compatibility of a seal with the fluids in a system is critical to obtaining a reliable, long-lasting seal. Here are some considerations for choosing the right material for a given chemical sealing application.
Polyurethane (PU) materials offer outstanding wear, extrusion and abrasion resistance with good elasticity and low compression set.
Looking Beyond Chemical Compatibility Charts: Matching Plastic and Elastomer Seals with Fluids
By Lucy Heyduk and Tim McCulfor, Trelleborg Sealing Solutions
Chemical compatibility charts are often used as a quick and concise way to match the proper fluid with a seal. However, there is much more to consider with the chemical compatibility of a seal in relation to the fluids in a system. This information is critical to gaining a reliable and long-lasting seal — and the selection process can be daunting.
This article was first published in Bulk Transporter.
Where the rubber meets the road for component design and manufacturing
The development of a custom rubber seal can be challenging.
Relying on industry specialists and considering potential manufacturing
methods and production volumes will enable you to navigate the
innovation process.
This article was first published in Design World.
Inventory Management Systems Play an Essential Role Now and Into the Future
As the economy reopens and demand for manufactured products returns to normal, it has become challenging to manage inventory of the parts needed for production. While no one product or service can solve all of these problems, inventory management systems have become an increasingly useful tool for managing labor and supply chain issues. This article reviews the current situation and how one new automated inventory management system can help alleviate some of the pain of C-Class inventory management.
From Deformation to Calibration: Installing O-Ring Energized Piston and Rod Seals
By Beth Figliulo and Michael Cook, Trelleborg SealingSolutions.
Avoid seal installation issues that lead to leaks and lost productivity.
Composite Simulation Grows MORE ROBUST
By Kenneth Wong
The transition from metal to composite is one of the most recent significant changes in manufacturing.
The former material is isotropic, exhibiting uniform stretching and bending behavior in all directions. By contrast,composites are anisotropic. They stretch, bend and break differently in different directions, based on how the fibers are woven together and how the laminates are bonded. This fundamental difference throws many traditional simulation protocols and practices into chaos.
Reduce Vibration and Avoid Stiction in Seals
By Holger Jordan, fluid power segment manager, Trelleborg Sealing Solutions
Stick-slip is not always a big issue, but sometimes it can significantly
degrade performance. Potentially, it can cause damage, such as cracks in
steel work and strength loss, and even health problems for operators.
We look at solutions to combat stick-slip to lower vibration as well as to create damping solutions.
When one is better than many
By Ursula Nollenberger; Trelleborg Sealing Solutions; Published in “MEDengineering” (edition 2/2020)
As medical devices become ever more sophisticated and smaller in size, the challenge for the component manufacturer is how to fit multiple functions into a limited space. Multi-component LSR technology offers a solution to this, that in addition, provides designers with the latitude and flexibility to enhance their applications.
By Michael Cook and Kelly Volpenhein; Published in "Fluidpower Journal"
This article was originally published in the February 2019 issue of Fluid Power Journal. It is reposted by permission.
LSR for Added Value Industrial Applications
With global engineering and production facilities, state of-the-art cleanrooms and advanced automated processes, Trelleborg Sealing Solutions already offers its medical device, biotech and pharmaceutical customers specialized custom molded solutions that enhance their product offerings.
By Beth Figliulo, published in "Hydraulics & Pneumatics"